12/18/2014 3:57 PM | |
Posts: 8946 Rating: (999) |
MMC is original SIMATIC and empty? |
12/18/2014 4:12 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating: (709) |
Hello Marysue, The CPU 300 without MMC not function, as said our expert IBN-Sevice the MMC is original Siemens? Have a look: Which memory cards can you use with an S7-300 CPU? How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? How do you reset a SIMATIC S7-300 CPU and MMC (default reset or overall reset)? |
12/19/2014 11:44 AM | |
Posts: 16 Rating: (0) |
Yes, the MMC is original, but not empty. I used it with a CPU 317-2DP. |
12/19/2014 9:25 PM | |
Posts: 16 Rating: (0) |
Is the MMC damaged the CPU? Is a new MMC can solve the problem of LED flickering |
12/20/2014 8:50 PM | |
Joined: 4/22/2010 Last visit: 12/13/2024 Posts: 5697 Rating: (715)
|
You wrote:
To me that means MMC is o.k. So CPU is dead or you are not following the right procedure, go for a Support Request Regards, Marcjan |
Problem solved? |
|
Follow us on