6/20/2014 3:27 PM | |
Joined: 4/30/2012 Last visit: 9/23/2024 Posts: 55 Rating: (1) |
Dear All I am using PCS7 V7.1 SP2 for my project. when I Open Alarm window in WiNCC Runtime the alarms are not displaing. In Status bar it is showing "All server onnection failed". I have enabled the Alarm and Tag logging option in my Project. Pls suggectthesolution. Regards Maddy AttachmentAll server connection failed.zip (214 Downloads) |
6/20/2014 6:39 PM | |
Posts: 2661 Rating: (279)
|
1. Run the OS Project Editor again (after deactivating WinCC RT). 2. Check in WinCC Explorer - Tools - Status of Client Connections. |
6/25/2014 8:48 AM | |
Joined: 4/30/2012 Last visit: 9/23/2024 Posts: 55 Rating: (1) |
Hi Yes U tried same project on another OS but same problem observed. Pls suggest. regards maddy |
6/25/2014 8:49 AM | |
Joined: 4/30/2012 Last visit: 9/23/2024 Posts: 55 Rating: (1) |
Hi YesI tried same project on another OS but same problem observed. Pls suggest. regards maddy |
Follow us on