7/7/2013 3:47 PM | |
Posts: 8946 Rating: (999) |
I = P / U P = U * I R = U / I |
7/7/2013 5:01 PM | |
Joined: 5/28/2008 Last visit: 12/17/2024 Posts: 4518 Rating: (841) |
Dear all, From the given data, all the above solution may be correct. Coz every body including myself put his assumption. kinjalpatel1899did not told us if it is 3 phase circuit or not. SoVithani'sAnswer is correct if it is 3 phase circut and ifkinjalpatel1899have some other loads connected with the capacitor bank. I mean if it is not a pure capacitor bank load. And in this case you need to know power factor. Navnaganswer is also correct if it is a pure capacitor bank. In this case Sin Phi = 1. So, I think thatkinjalpatel1899have to clarify these points or go through thislink |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on