4/15/2013 2:38 PM | |
Posts: 27 Rating: (0) |
i have Analog input module 2AI x I, 2-wire how to scale input 4 -20ma in program? in put is vfd 7.5 hp. |
6/27/2013 6:55 PM | |
Posts: 93 Rating: (13) |
Dear friend, Your input is used for VFD current or speed feedback?? |
7/16/2013 1:54 PM | |
Joined: 5/28/2013 Last visit: 2/1/2023 Posts: 112 Rating: (3) |
With this library you cans easily scale analog inputs: |
7/16/2013 4:39 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, you can refer following FAQ's too. For Simatic Manager How and for which analog measurements can you use the function FC105 "SCALE" to convert the integer values (INT) into real number values? For TIA Portal In STEP 7 (TIA Portal) V11, how can you scale integer values in real numbers and real values in integer numbers for analog measurements? For Microwin How can you scale analog values with S7-200 in conjunction with CPU224XP and expansion modules EM 231, EM 232 and EM 235? |
VANDE MATARAM..... |
|
2/12/2014 9:11 AM | |
Posts: 27 Rating: (0) |
thanks all dear friends, |
Follow us on