4/30/2019 2:24 PM | |
Joined: 10/16/2007 Last visit: 2/23/2024 Posts: 627 Rating: (45) |
Hello, can you upload the program? Without it is difficult to check what will happen. Regards |
5/2/2019 11:51 AM | |
Posts: 66 Rating: (1) |
Hay ifte, U may need to share your program with us |
5/10/2019 9:04 AM | |
Posts: 2826 Rating: (684) |
@crazyCow - You may want to know about SHRB instruction that is available in the library section (if remembering correctly). As I do not have Step7 Classic, I will not be able to tell you & ifte exactly where the instruction is. The attached PDF has been generated from TIA Portal. I think there is no need to have more than one shift register. The one pulse says yes/no and the other gives timing (when to shift). The position in the shift register dictates which action is required. Attachmentshift-bit-register.pdf (177 Downloads) |
Last edited by: #dP at: 05/10/2019 09:06:05 |
|
This contribution was helpful to1 thankful Users |
Follow us on