3/9/2020 6:27 PM | |
Joined: 8/15/2019 Last visit: 9/23/2024 Posts: 4 Rating: (0) |
Hi to all, We have one application with CPU 1513R-1 PN, redundancy, we passed all manuals unfortunately without any positive result, Current configuration: CPU 1513R-1 PN (6ES7 513-1RL00-0AB0, V2.6) x 2 pieces, SCALANCE X204 IRT (6GK5 204-0BA00-2BA3, V5.3) x 1 piece Profinet encoder 6FX2001-5xN13 single turn, CU240E-2 PN (6SL3244-0BB12-1FA0, V4.7.10) The task is to make a ring with two PLC-s and have client devices, one encoder and G120 drive. In a hardware configuration, we can't add in the same network all devices. from the manual, we tried to add ET200 IM155-6 PN HF and IM155-5 PN HF and in HW compile pass without any error, but unfortunately, we don't have these modules to test application in real-time application. in our configuration with eth. switch and other devices, we don't get status: "Multi assigned", we can connect just one PLC at the same time, primary or secondary, not both. probably this device isn't supported for redundancy, but for the switch is noted that can be redundant. Compiled always return the error: "The configuration of the device "Drive_1" contains one interface module assigned to one PLC (S1 configuration). This is not supported by the controller "PLC_1".,,,3:14:27 PM" we would like to make some similar configuration what I attached with S1515R but without ET200 modules. And the difference is that we have S1513 CPUs... is it possible somehow to connect Profinet encoder and G120 driver, or we need to put one 'normal PLC' as we made in the example? in the example in attachment is one another configuration with network ring, but that is something much different than ring what we want to make with S1500R. Is it possible that Siemens support just these few modules in redundancy configuration: (because with this modules HW configuration working fine) 155-6AU01-0CN0 155-6AU30-0CN0 155-5AA00-0AC0 158-3AD10-0XA0 3040-1LA01-0AA0 3040-1MA01-0AA0 Thank you in advance Elvis,. ------------------------------------------------------------------------------------------ AttachmentSIEE.zip (390 Downloads) |
Last edited by: CS Moderator at: 03/10/2020 09:29:33New subject after splitting |
|
Follow us on