11/10/2022 8:30 PM | |
Joined: 3/14/2008 Last visit: 11/9/2024 Posts: 2124 Rating: (951)
|
Hi, In paragraph 20.7 you can see the 414-4H and 417-4H. Both are released for PCS7 V9.1 SP2. The code "W" means that the module wizard is support (the communication between hardware and software basically) and "X" means that the station can be used with CiR (Configuration in Run) components. Please bear mark that you will need the exact same MLFB number and check if you have the firmware as described. Lower firmware versions can get you in trouble. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on