2/9/2012 9:47 PM | |
Posts: 21 Rating: (0) |
Dear all: This is my problem... I´m migrating a PCS7 V6.1 + SP2 based control system to PCS7 V7.1 + SP3, but, I´m using AP Library, during functionality test period everything was working Ok, but on the plant, when the program download was performed, on the stop-run transition the cyclic time overpassed the 6000 ms watchdog time, going up to 24000 ms, and the mean time goes up to 1450 ms... The test were made over a 417-4HT14 CPU, but the plant AS works on a 417-4HL04 CPU... On the attached file are the main CPU images of the Module information, such as Diagnostic buffer, Scan cycle time and memory. Also are included the images from the OS diagnostics, showing the ciclyc failures. Also included the logs form compilation, download & module driver information... I hope this info be enough to make some diagnostic. Thank you in advance.
AttachmentFalla CPU.zip (81 Downloads) |
2/13/2012 9:48 AM | |
Joined: 10/26/2011 Last visit: 11/11/2024 Posts: 762 Rating: (192) |
Hello Luis, |
SIMATIC PCS 7 - Overview |
|
Follow us on