6/23/2020 4:19 PM | |
Joined: 2/1/2010 Last visit: 8/7/2024 Posts: 149 Rating: (71) |
Hi AMAZINGAHMED In general you can use the normal PO calculation guidelines and estimate your logic. How are the licenses for the AS and OS counted in PCS 7 V7.0 onwards? Extra considerations related to safety: Do you plan to use Safety Matrix or just create your own custom yellow code in CFC? If using Safey Matrix and enabling alarms for causes/effects, then each cause/effect with messaging enabled counts as a PO, in addition to the matrix. So don't forget to count those in the calculation. If you are doing just your own custom logic, then you'll have to default back to the manual counting as defined in the link. AS SEC PO just needs to be unlocked higher than your AS PO count. So you if you calculate 1150 AS RT PO for example, then you need a AS with AS SEC PO unlocked to 1200 per controller. (so you can order AS 1000 bundle and add 200 extra per each controller - if redundant this means you need to order 4x 100 adders) Or you can order AS 1600 bundle and have more spare capacity. |
Last edited by: RVS.wick at: 06/23/2020 16:20:24Last edited by: Jen_Moderator at: 06/24/2020 09:16:04Optimized link. If my post helped you, please rate. Thanks. |
|
This contribution was helpful to1 thankful Users |
6/24/2020 1:00 AM | |
Joined: 2/1/2010 Last visit: 8/7/2024 Posts: 149 Rating: (71) |
Based on my calculations I think your numbers are slightly off. I remember having a lot of trouble estimating early on as well. For my own experience and some historical word of mouth from various other experts I use these rules which can relate to the official method but is less accurate. (It will not be 100% accurate, but it will be close enough to buy licensing on most projects.) Using APL or APL like blocks: 1 controllable object = 1 AS PO +1 OS PO (APL object block like MonDiL, not Intlk04, or OR4) Case 1: Using CFC safety blocks
Case 2: Using Safety Matrix
If you actually build Case 2 in a totally blank test project the actual PO usage is 12 AS PO and 11 OS PO, so I think my safety baseline estimate is slightly off or there are other blocks I've just never accounted for which are maybe part of the non-safety compiler setup. However it will scale up from there if you add more causes/effects to the same matrix according to the estimate methods. Maybe another expert can find the hole in my estimation but this is typically good enough for order of magnitude. In my experience you never want to be right up against your PO limit because the customer/user will always ask for one more thing. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to3 thankful Users |
Follow us on