7/11/2017 8:32 AM | |
Posts: 11 Rating: (1) |
Hello boycemento, no it won't. For further information you can read this detailed industry support documentation of SIEMENS: Documentation for PCS 7 V8.1 I hope I could help you. Regards, !PCS007! |
Last edited by: !PCS007! at: 7/11/2017 8:50:53 AMLast edited by: Jen_Moderator at: 7/11/2017 9:44:37 AMEdited post for better reading |
|
7/11/2017 9:47 AM | |
Joined: 4/22/2010 Last visit: 5/19/2023 Posts: 82 Rating: (1) |
Thank you so much..i'll check the link later... |
7/11/2017 11:13 AM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Here the link to the current manual "CPU 410 Process Automation": |
Last edited by: Thunderstorm at: 7/11/2017 12:39:21 PMLast edited by: Thunderstorm at: 7/11/2017 12:40:24 PMSIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
8/15/2017 1:52 AM | |
Joined: 4/22/2010 Last visit: 5/19/2023 Posts: 82 Rating: (1) |
Dear Thunderstorm, I went onsite yesterday to upgrade the SE PO of the 410 CPU but found out later that online SE PO upgrade is only possible with PCS7 Version 8.1 or higher. The problem is that , they are using PCS7 V8.0 . Below are the things I've observed yesterday: 1. I’ve have tried to check the license key using my laptop and found out that there is a license inside. Im using a virtual machine with PCS7 V8.2 installed. The “connect target system” option is also available on ALM. 2. But when we used the same license key usb on their Engineering Station, we got a different response. The ES can’t see what’s inside the license key USB. The “connect target system” option is also not available on ALM Is there any work around or other solution to this issue without upgrading the system (PCS7 version upgrade)? Were planning to upgrade the SE using my laptop but I'm not sure if will still have compatibility issues since they are using a lower version of PCS7. Kindly see attached files for your reference. Hope you can help me with this. Thank you in advance. Best Regards, Boycemento AttachmentSE PO UPGRADE.zip (99 Downloads) |
Follow us on