4/25/2023 6:44 AM | |
Joined: 11/22/2021 Last visit: 5/6/2024 Posts: 2 Rating:
|
Hello, I am facing the same problem with WinCC 7.5 + SP2 on Windows 10, After PC reboot, autostart doesnt work as usual. First error after reboot: The system cannot find the file specified, after clicking OK (no other option), i get another error: No connection to script control then i click OK (no other option) as well. After 30 seconds Autostart starts the runtime application as always, but if i dont click on "OK" on mentioned errors then runtime stops in 75%. This behaviour is not acceptable, i just want Autostart work properly without errors and without operator need to click on errors. Can anybody help me please? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/25/2023 11:03:01New subject after splitting |
|
Follow us on