11/5/2009 4:39 PM | |
Posts: 45 Rating:
|
I have not done any project with WinCC Client but i guess is almost the same as the server. If u close WinCCExplorer and the application is running it will automaticlly start up the runtime when u start WinCCExplorer. So to make WinCCExplorer start up automaticlly u have to create a shortcut of WinCCExplorer.exe and put in "Start > All Programs > Startup" So next time u start up the computer it will automaticlly start WinCCExplorer.exe witch in turn start runtime if it was allready running last time WinCCExplorer was shut down. For automatically logon there is the way that u have createt windows logon user "Simatic Logon" Then u can use this guide http://www.mydigitallife.info/2008/01/15/auto-login-to-windows-without-entering-password/ If u are not using Simatic logon then i dont really know :S perhaps with a script? Maybe there is something in this pdf file. GL!AttachmentUserAdmin.pdf (383 Downloads) |
11/6/2009 8:07 AM | |
Posts: 133 Rating:
|
It helped! I didn't knew that I can add to autostart "remote" project... Thank you. |
11/6/2009 9:23 AM | |
Posts: 22 Rating:
|
Hello If you will make auto Logon, look after "Silent Logon" from PCS7, I use it in standard WinCC app. |
10/19/2015 3:33 PM | |
Posts: 288 Rating:
|
Dear experts, i am waiting for your reply. thanks. |
Follow us on