7/13/2016 12:02 PM | |
Joined: 11/29/2011 Last visit: 5/1/2024 Posts: 1356 Rating: (229) |
Hi, I was asked about an error occurred during a changes only download in CFC. The error says: E: Block FC1736 does not exist. Please copy it to the offline block folder! See the attached zip file for information. I performed a MRES on the CPU to make sure it is not the result of something left in the CPU from previous tests. It did not help. I checked out the Block folder and these FC's are missing and seem to relates to Runtime group. Any idea about how to clear the error? AttachmentPLCFI2C_ChangesDownld_FC_Errors.zip (70 Downloads) |
- What you read here, please check with manuals and your requirements. |
|
7/13/2016 2:21 PM | |
Joined: 11/29/2011 Last visit: 5/1/2024 Posts: 1356 Rating: (229) |
Hi, I have tried that. Did not help. I am looking at the logs. I am wondering if it is anything to do with the local data stack/priority classes. See the attached logs. AttachmentPLCFI2C_ChangesDownld_FC_Errors_2.zip (49 Downloads) |
- What you read here, please check with manuals and your requirements. |
|
7/14/2016 12:46 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Microman, Very strange indeed. With the "Update Block Types" function, you can delete unused blocks from the CFC charts, but also delete unused blocks from the "Blocks" folder or both. What I want to ask if you were aware of this? I also had this problem once, but was solved with the Update block types. Maybe "Reorganization with slow" would have helped? But, I'm very curious what you found out about this error. |
If I could help you, you can use the RATE button. Thank you. |
|
7/14/2016 2:28 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Microman, Ah ok, I had this once, where I only deleted the block from CFC charts, but not from Blocks folder, so I thought this was OK, but it wasn't |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on