Industry Online Support
Technical Forum
12/8/2010 3:53 AM | |
Posts: 1 Rating: (0) |
Dear mr, I have an system with CPU314-2DP with 2 station : 1 IM153-2 (6ES7153-2BA01-0XB0), 1 fanuc station Now, when I turn off and turn on the CPU. Time for booting system is too long about 2 hours (in this time the system display : bus1 fail ) I tested the IM153-2 modul, the profibus cable, the comunication port on the cpu by BT200 (Siemen test tool) and is said all are ok do you know what wrong with It ? and how to solve that problem Attachmentminhphong_1.zip (46 Downloads) |
12/8/2010 5:17 AM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359) |
Dear member Please follow the diagram shown in the attachment to connect the cables to the PROFIBUS connector .Then, In hardware configuration station-> online check if the slave is available or not? regards Attachmentimg515.zip (73 Downloads) |
8/6/2011 6:40 AM | |
Posts: 4 Rating: (0) |
Hi please send this file to me, i cant download it, i dont know why!? Mostafa |
Last edited by: CS Moderator at: 8/7/2011 11:08 PMContact data deleted |
|
Follow us on