11/29/2023 6:45 AM | |
Joined: 2/22/2006 Last visit: 2/17/2024 Posts: 73 Rating: (3) |
Hi Georg, we are dong a migration from WinCC 7.0 to 7.5, in the project ukrainian is used, so we have cyrillic texts. If i do the migration with "Ukraine", also the C-Scripts are ukrain and not "dynamic", if I use "Englisch USA" the texts are damaged. But what is the really the problem, if the c-scripts setting is ukraine? Or how can I have both, C-scripts dynamic and correct texts? BR ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/29/2023 13:30:24New subject after splitting |
|
11/30/2023 10:02 AM | |
Joined: 8/3/2009 Last visit: 5/24/2024 Posts: 12981 Rating: (1653)
|
Hello Icebear17 ---- The Microsoft C compiler used in WinCC does not support Unicode. Therefore, ---- https://support.industry.siemens.com/cs/ww/en/view/44029132 Hope this information helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on