2/15/2017 8:12 AM | |
Joined: 5/8/2016 Last visit: 2/15/2024 Posts: 167 Rating: (13) |
dear all engineers and expert : i need to take a back up from siemens panel with part number 6AV6 642- 0AA11-0AX1 the problem appears when i try to connect by prosave v13 (no connection established ) i tried by MPI PC adaoter cable and PPI cable but nothing happened .... could you recommend me the best cable to connect ( PC adapter ) or (PPI CABLE ) and the appropriate prosave version and the appropriate procedure
thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/15/2017 1:32:05 PMNew subject after splitting A lot of potential remains |
|
2/16/2017 8:18 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, Attached a file that will tell you which cables to use with any Simatic Panel. Attachment19109408_wincc_flexible_projekttransfer_e.xlsx (467 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
2/20/2017 10:16 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, Yes you are right. Delivery Release: 90° Angle Adapter - 9-Pin RS 232/RS 422/RS 485, and RS 422/RS 232 Converter |
Ayman Elotaify |
|
2/20/2017 10:54 AM | |
Joined: 5/8/2016 Last visit: 2/15/2024 Posts: 167 Rating: (13) |
Dear eng Ayman can i use reguler serial 9 pin cable with USB to Serial convrter without needing to use this siemens right angle adapter ??? thanks in Advance |
A lot of potential remains |
|
2/20/2017 11:22 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating: (839) |
Hello, I have never tried this solution and I don't think it will work. As it is not written in the excel sheet attached in prev. post. You should select in Prosave or WinCC flexible the cable you already connect to your Panel. And you will not found a selection with a serial - USB converter. |
Ayman Elotaify |
|
Follow us on