8/13/2018 11:30 AM | |
Posts: 19 Rating:
|
Hi again, So I now builded the image and it worked fine no errors and so on. I also added the conf settings for uvcvideo but when i boot the iot and connect the camera there is no /dev/video* ore something like this. So I don´t think uvc is succsessfully enabled. Is there any driver I have to install to? I also tryed modprobe uvcvideo but of course there is no uvcvideo.ko file do I have to create such a file or something like this? Or is there something else I have to do am I missing something? I did following until now: 1) builded the stnadart image with kas 2) added the required config settings to a new .cfg file and includet this file to the linux-cip_4.4.bb file. (also tride to add the settings directly in defconf) the cfg file includes following: CONFIG_VIDEOBUF2_CORE=m 3) rebuild the image with the bitbake command 4) wrot the image to a SD card and booted it up everything works but uvc don´t Kind regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/13/2018 1:44:15 PMNew subject after splitting Last edited by: AutoGen_9015344 at: 8/14/2018 4:03:55 PM |
|
Follow us on