4/19/2022 10:29 AM | |
Joined: 8/19/2011 Last visit: 4/2/2024 Posts: 3 Rating: (0) |
Hello, I think I have the same problem (I think). I am using a ET200SP (CPU1512SP F-1 PN) an a HMI MTP1900 Unified Comfort Panel. Sometimes, I have to use a VPN Connection, an then, I can not see the HMI "Online". I can not connect or find the HMI an I can not see the "Online and diagnostics" Page. When I have a activ connection to the PLC, I can update the HMI Programm, but only the Software and I can not make any diagnostics or Operating System Updates. Why can I use and connect the PLC, Servo Drives .... but not the HMI? What is the difference between this connections? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/19/2022 13:48:06New subject after splitting |
|
4/20/2022 10:27 AM | |
Joined: 8/12/2021 Last visit: 4/16/2024 Posts: 303 Rating: (28) |
Hi N. Moldenh! Is the system updated to the latest version? Firmware? This link may help. |
If this Information really helps, you could use the Rate function |
|
Follow us on