3/17/2021 7:31 PM | |
Joined: 2/25/2021 Last visit: 11/2/2022 Posts: 73 Rating:
|
Instead of connecting LOGO1 to LOGO2 in the Network Project window, can we set LOGO1 as a client and LOGO2 as a server in Ethernet Connections? In that case, when entering the client connection, how do we transfer the information from NQ1 to NI1? How many bytes do Q and I hold? Thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/18/2021 09:25:03New subject after splitting |
|
3/17/2021 8:36 PM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
You can also connect two LOGO!s with each other in diagram mode without any problems. See attachment. Take a look at the ethernet connections. I didn't understand the question about the I /O, so you have to explain more.
AttachmentClient_Server.zip (294 Downloads) |
This contribution was helpful to
1 thankful Users |
3/18/2021 9:45 AM | |
Joined: 12/18/2014 Last visit: 7/25/2024 Posts: 33414 Rating:
|
For better understanding ...
AttachmentLOGO! Bit, Byte, Word and DWord.pdf (326 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on