4/7/2021 10:38 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
well, thanks for trying to help me. i can't connect remote IO(such as simatic ET 200MP) to the main cpu in TIA selection tool, only communication modules ,analog I/O,DIO inside the controller. i can't choose both of them [snip] there is a problem with PLCSim, you can't simulate every thing ------------------------------------------------------------------------------------------ |
Last edited by: engco at: 04/07/2021 22:39:01Last edited by: engco at: 04/07/2021 22:41:18Last edited by: engco at: 04/07/2021 22:42:41Last edited by: Jen_Moderator at: 04/09/2021 06:31:58New subject after splitting. Added embedded image as an attachment. |
|
4/9/2021 4:36 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
If I choose controllers then choose plc there is no way to choose IO |
4/10/2021 2:13 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
if i want to connect more than one remote IO to the main plc, will i need a communication switch? |
Follow us on