3/1/2018 11:51 AM | |
Joined: 1/13/2016 Last visit: 8/29/2022 Posts: 37 Rating: (0) |
Hi, thank you, I've already fixed it. But I faced an other problem, I have a Server/Client setup. The runtime in my server (ES+OS server) is running well, but my other station (OS Client + Open PCS7 station) is not. I can't download the Client station from the Server ("rt station not obtainable"). I can ping this station, I can share and copy manually. Do you (or somebody else) have any idea for this problem? Thank you! Kopo ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/1/2018 12:36:08 PMNew subject after splitting |
|
2/21/2020 8:18 PM | |
Joined: 4/28/2017 Last visit: 10/3/2024 Posts: 149 Rating: (24) |
Hello kopo_vagyok: What did you see when you said checked Simatic Shell? Did you notice the Client computer name on the Simatic shell list? Please check the following, In your client PC, If the windows firewall is on, turn it off and check again. And, if you have installed any antivirus, please turn it off all of its actions (Over network firewall), You should be able to see that client PC name in your ES Simatic Shell, if not still then verify your "Lmhost.dll" file in windows. (But, You must select your terminal bus adapter in the settings tab of Simatic Shell) keep your PG/PC settings in "PC internal" and ensure have properly configured the station configurations. |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on