5/14/2020 6:15 PM | |
Joined: 2/5/2013 Last visit: 5/9/2024 Posts: 320 Rating: (74) |
Hi mkorpecki, You can put support request to Siemens. Br, AmolG |
Please rate it. |
|
5/14/2020 6:28 PM | |
Joined: 12/18/2014 Last visit: 5/12/2024 Posts: 33020 Rating: (4079) |
I think that the CPU is to old for the actually software ... |
5/14/2020 6:51 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2667)
|
Hello mkorpecki; This manual is dated 2001, and it does not contain anything on a CPU 314-1AC00- 0AB0. https://cache.industry.siemens.com/dl/files/591/8860591/att_105766/v1/HB_CPU312IFM_bis_318-2DP_e.pdf There is no link to that part number either in the Industry Mall, the S7-300 refurbisher shops on the web (those that present such a part number all show "not available" or "call for a quote", which means...), or on specialized sites on datasheets and manuals. So, either it is really, really obsolete as ixo65 said ( and no longer supported even by Step 7 v5.x), or you will have to follow AmolG's recommendation to attempt a Support Request to ask a Siemens tech (link at the top of this page). Or... you could make sure about this part number on the CPU. The markings on the front bezel sometimes get erased over time, but the ones on the side of the modules generally are preserved. Could you remove the CPU from the rack and take a picture of the label you will find there? Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
5/14/2020 8:12 PM | |
Joined: 4/12/2019 Last visit: 11/8/2021 Posts: 9 Rating: (0) |
At the photo you can see part number and I'm sure about that is 6ES7 314-1AC00-0AB0. Is this possible that this PLC is chinese fake? |
5/14/2020 8:23 PM | |
Joined: 2/5/2013 Last visit: 5/9/2024 Posts: 320 Rating: (74) |
Hi mkorpecki, From my point of view In some special cases and as per request from OEM to protect there data from copy protection siemens develops some special products which are normally not available for normal user.If possible put service request Br, AmolG. |
Please rate it. |
|
Follow us on