6/24/2013 11:18 PM | |
Joined: 2/5/2009 Last visit: 3/19/2024 Posts: 36 Rating: (1) |
Hello all, Someone can help me?? I'm trying install the setp7 v11 in my laptop (DELL PRECISION M6400) without sucess. The operation system is XP PROFISSIONAL SP3. When I start the installation the window in figure(image 1) in attachement close automatically and the installation stop. I send in attachement the log files. Thanks AttachmentStep7 v11.zip (150 Downloads) |
6/25/2013 11:15 AM | |
Joined: 2/5/2009 Last visit: 3/19/2024 Posts: 36 Rating: (1) |
Hello Huggy_d1 Thanks for your repply I'm using DVD witch contain Step7 Portal V11 SP2. |
6/25/2013 11:50 AM | |
Joined: 4/17/2012 Last visit: 3/30/2024 Posts: 474 Rating: (10) |
Hi, copy the DVD and paste the execution files in ( D:\ Or E ,)some other drive then run the installation procedure... please check this path any file u have already ???? C:\TEMP\STEP7_PROF_V12\sia.cfg Already you are having TIA V 12 ????... anytime before you used this lapyop with TIA 12??????
|
6/25/2013 12:19 PM | |
Joined: 2/5/2009 Last visit: 3/19/2024 Posts: 36 Rating: (1) |
Hi, copy the DVD and paste the execution files in ( D:\ Or E ,)some other drive then run the installation procedure... I try install by an external disk and have the same problem. please check this path any file u have already ???? C:\TEMP\STEP7_PROF_V12\sia.cfg I cheked and I dont have the file Already you are having TIA V 12 ????... No anytime before you used this lapyop with TIA 12??????
No Thanks |
6/25/2013 12:45 PM | |
Joined: 4/17/2012 Last visit: 3/30/2024 Posts: 474 Rating: (10) |
in this post also same installation issue pls check it |
6/25/2013 3:30 PM | |
Joined: 7/7/2010 Last visit: 5/14/2024 Posts: 14722 Rating: (2363)
|
Do you have admin rights to install the portal software with the login account you are using? If not, can you login to a different account with admin rights and try again? If you have admin rights and everything else meets the required specs (free drive space, system memory -- at least 4GB is my suggestion), you may want to contact Siemens via Support Request |
science guy |
|
6/25/2013 3:55 PM | |
Joined: 2/5/2009 Last visit: 3/19/2024 Posts: 36 Rating: (1) |
Thanks I will request siemens support |
Follow us on