2/22/2012 1:06 PM | |
Posts: 63 Rating:
|
Hello all, AttachmentInterface_PG_OP.zip (223 Downloads) |
Last edited by: Rosegarden at: 2/22/2012 2:18 PMLast edited by: Rosegarden at: 2/22/2012 1:19 PM |
|
2/22/2012 4:18 PM | |
Posts: 63 Rating:
|
Hello Darius and Marcjan, thans alot for the helpful info, sadly enoughIstill can'ttranferthe project from the PG to the OP. I have includedsomepic's aboutthe interfaces, I can;t seeanything wrong about it but can youplease take a look atit ? The DIP switches are set for Profibus DP, so they're all set to MPI/DP/PPI. Thanks in advance. AttachmentInterface.zip (175 Downloads) |
2/22/2012 6:07 PM | |
Posts: 3037 Rating:
|
Hello, You have wrong settings in the PC/PG interface. You must use Profibus DP in your PC/PG interface. You have a connection via Profisbus DP from Panel to PLC. You can see more information about download via Profibus/MPI in the following FAQ. How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Tweety |
This contribution was helpful to
1 thankful Users |
2/23/2012 1:44 AM | |
Posts: 98 Rating:
|
Just to make it easier to use LAN port. more simple. Only setting IP Address
|
Follow us on