9/9/2019 2:13 PM | |
Joined: 4/2/2016 Last visit: 7/13/2022 Posts: 413 Rating:
|
first of all DRIVE-CLiQ signal cables has two types -Pre-assembled DRIVE-CLiQ signal cables (without 24 V DC cores) - DRIVE-CLiQ MOTION-CONNECT 500 signal cables (with 24 V DC cores) it is clear, DriveCliq encoder requires external power, so original DriveCliq Cable has additional power wires. But what for example, if we need to connect CU320 and SLM (SMART LINE MODULE) SLM and SLM CU320 and SMM (SINGLE MOTOR MODULE) CU320 and TM31, SMC30, TM150 in these cases, can use the standard patch cords (no DriveCliq)??? Of course it is better to use the original but for example if i ordered the wrong length (not enough length)... ------------------------------------------------------------------------------------------ |
Last edited by: _oleksandr_ at: 09/09/2019 14:31:21Last edited by: Jen_Moderator at: 09/10/2019 06:09:57New subject after splitting |
|
Follow us on