4/24/2012 12:05 AM | |
Posts: 2 Rating: (0) |
good day can you control 4 servomotors with S7200 plccommunication via Profibus?
|
4/25/2012 6:53 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello philiperalta; This extract from the S7-200 System Manual can give you basic information for your project: Basic Information for Open Loop Position Control UsingSteppers or Servos Both the PTO built-in to the S7-200 PLC and the EM 253 Position Module use a pulse train output to control both the speed and position of a stepper motor or a servo motor.Using the PTO or the module for open loop position control requires expertise in the field of motion control. This chapter is not meant to educate the novice in this subject. However, it provides fundamental information that will help as you use the Position Control wizard to configure the PTO or module for your application. http://support.automation.siemens.com/WW/view/en/1109582 Study the chapter on Open Loop control for more details. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 4/25/2012 6:53 PM |
|
Follow us on