10/19/2018 10:14 AM | |
Posts: 4 Rating: (0) |
Hello, i've try both solution but from my app based on Sharp7 i cannot connect to my s7200. I've need to set something inside the project in microwin? Then compile and resend it to plc ? Autogen and bojanor code return me error 5 one the connectTo or Connect function. Please can anyone help me ? Thanks a lot ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2018 11:17:31 AMNew subject after splitting |
|
10/19/2018 5:50 PM | |
Posts: 4 Rating: (0) |
Duris in my real code i try to Connect to IBH ip. ip are ok, the code that i post is only for example. |
Follow us on