5/9/2022 4:45 AM | |
Joined: 4/14/2017 Last visit: 1/3/2023 Posts: 9 Rating: (0) |
Please mention what you did to create process cell. I followed all the steps with BATCH example project, assigned role Logon_Administrator for Superuser so all permissions were available. However, I cannot create process cell or any major functions. I reinstalled several times but still not OK! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/09/2022 12:27:49New subject after splitting |
|
5/10/2022 4:05 PM | |
Joined: 2/17/2020 Last visit: 4/30/2024 Posts: 994 Rating: (169) |
Hello again, Please review the following section of the manual: "Users intended to use SIMATIC BATCH must be added to the members of the "SIMATIC BATCH" and "SIMATIC HMI" Windows groups. Only then can you assign the relevant roles for SIMATIC BATCH to these users in the SIMATIC Logon roles management (Options > Roles management in the BatchCC). SIMATIC BATCH V9.1 - Specifying user permissions Is this user in the Windows groups "SIMATIC BATCH" and "SIMATIC HMI"? |
A rating will be well appreciated. |
|
5/11/2022 5:27 AM | |
Joined: 4/14/2017 Last visit: 1/3/2023 Posts: 9 Rating: (0) |
I added memberships as you mentioned but nothing happened. The menu to create new process cell is still greyed out |
5/31/2022 9:03 AM | |
Joined: 1/11/2019 Last visit: 4/30/2024 Posts: 702 Rating: (140)
|
Hello Dat_BK, Continuation with forum users guidance, I would like to add two more points. Point 1: Kindly check whether you have configured Batch Application and Batch application client. If it is not configured then, You can not create process cell even though you have higher level of authentication. (Configuration.png) Point 2: Open Batch control center and check whether process cell is already present. (If yes, You can not create one more process cell(BCC.png)) Note: .png files are in Snapshot.zip file I hope it helps you! AttachmentSnapshot.zip (380 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on