5/4/2020 2:27 PM | |
Posts: 2 Rating: (0) |
Dear All, I have similar problem with my new PC Adapter USB A2 (6GK1571-0BA00-0AA0). I already installed PC adapter driver on my Window7 Pr 64 Bit OS and my OS recognize the adapter correctly. Also I set my PG/PC interface in Step 7 v5.5 + SP4 correctly (MPI, station address is 0, timeout is 30 seconds, speed is 187,5 kbps and highest station address is 31). However I am able With the old PC Adapter (6ES7 972-0CB20-0XA0) everithing is working correctly and without any problems but with new one i cannot establish connection with CPU (S7-414 2DP) via MPI (Note that all settings are completely the same as in case of old adapter). Can you please suggest any solution how can I solve this problem ??? Regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/05/2020 07:41:50New subject after splitting |
|
5/5/2020 6:19 AM | |
Posts: 2 Rating: (0) |
SIMATIC PC Adapter USB A2 ( 6GK15710BA000AA0 ) not connecting to PLC. Attached message coming.. |
Follow us on