6/10/2022 10:13 AM | |
Joined: 12/10/2021 Last visit: 1/3/2023 Posts: 2 Rating: (0) |
Hi everyone, I've encountered the error described below, prohibiting chart compilation. Any assistance would be greatly appreciated. Problem description: When compiling CFCs from Component View, an error occurs during module driver generation. A pop-up with the following content is shown: Generate module drivers (1739:260) From the “Module driver” tab of the Logs dialog box, a description of the underlying problem can be found: E: Could not determine insert points of block FB_In. The insert positions were not modified. Clicking on the “Go To” button for this error opens the CFC: Interconnect Blocks window with the same “Cannot read hierarchy folder” pop-up, but no chart is opened. (Hence, we cannot determine what FB_In is.) Detailed information: 1.Urgency (Technical question or Immediate) Immediate 2. PCS7 version (incl. Service pack, Update version). Also write down if updates are installed for separated products (for example: WinCC, CFC, SFC etc.) PCS7 version: V5.6 + SP2 + HF8 3. Operating system (incl. Service pack) VMware Workstation 16 Pro running Windows 10 Pro (version 21H2) 4. Is the application migrated? If yes, from which version? No. 5. How often does the problem happen (Always/Often/Once/Not applicable)? Always 6. Is there a workaround? None found yet. 7. Did the function/functionality previously work? If yes, did something change recently (Windows update, PCS7 update etc.)? Control Module Types (CMTs) were changed, but compilation works on a colleague’s VM. 8. MLFB number (in case it applies to hardware) N/A 9. Firmware version (in case it applies to hardware) N/A Thanks for your time! Attachmentsupporting-images.zip (299 Downloads) |
Last edited by: stef_coetzee at: 06/10/2022 10:15:30 |
|
6/10/2022 6:30 PM | |
Joined: 12/10/2021 Last visit: 1/3/2023 Posts: 2 Rating: (0) |
Thanks to all for the responses. I've since narrowed the issue down to a handful of charts that somehow remain behind after the area of the plant they belong to is deleted. Since the area has been deleted from the Plant Hierarchy View, they no longer belong to an area. Under Charts in the Component View, for each of these charts, the entry under the "PH Assignment" is "---". See context image #1. Is there a way to remove these charts? When attempting to delete them from Component View Charts (right-click > Delete), an error message is shown. Message content (context image #2):
After that a system error pop-up details which functions are failing (context image #3). An update to point 6 in the original post of this topic: 6. Is there a workaround? Yes, keep problem charts in project hierarchy instead of attempting to delete them. Note: Reorganization (using the "Save As with Reorganization (slow)" route) failed with the message:
Deleting the @-prefixed charts are likely not the problem. Instead, I suspect these charts that remain behind without plant hierarchy after the plant area they belong to is deleted are the cause of the plant-hierarchy error. Attachmentcontext-images.zip (330 Downloads) |
Last edited by: stef_coetzee at: 06/10/2022 18:31:10Last edited by: stef_coetzee at: 06/10/2022 18:32:16Last edited by: stef_coetzee at: 06/10/2022 18:34:22Last edited by: stef_coetzee at: 06/11/2022 18:17:38Last edited by: stef_coetzee at: 06/11/2022 18:25:01 |
|
6/19/2022 6:49 PM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150)
|
Hello Stef_coetzee, Sorry! Could not give you the solution from myside Kindly rise a service request using below link |
Follow us on