4/25/2010 5:48 PM | |
Joined: 4/24/2010 Last visit: 1/24/2024 Posts: 16 Rating: (0) |
I arleady connect PLC 224 to MM410(ON OFF1 OFF2 Change dir ok.But when i use USS_WPM_W to change value in P2000 i MM410 it does not effect P0003=3 P1000 Index 0=5 P2009 Index 0=0 Attachmentuss.zip (45 Downloads) |
4/26/2010 8:06 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Connect PLC 224 to MM410 Use USS Protocol???. Best regards O_Moderator |
Follow us on