4/15/2020 11:32 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating:
|
Hi CEMAT blocks should be called in OB1 rather than "normal" PCS7 blocks. Normal I mean like APL library and old classic V7.1 blocks. You can change the blocks by the following: 1. Open CFC and press Ctrl+F11 or go to Edit->Open Run Sequence. On the left hand side you can see all OB's and blocks in them. You can drag and drop or select multiple blocks/runtime groups and place them in another OB, in your case OB1. |
If I could help you, you can use the RATE button. Thank you. |
|
4/16/2020 9:05 AM | |
Joined: 3/14/2008 Last visit: 9/12/2024 Posts: 2095 Rating:
|
Well, There is not much info about these faults. You can check however the following: Your blocks/groups should be placed between runtime group OB1_START and OB1_END. Can you check this? See attachment. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on