1/20/2021 2:48 PM | |
Joined: 11/8/2017 Last visit: 8/13/2024 Posts: 328 Rating:
|
Hi, You can add an additional language using the 'Update Desigo CC' shortcut that should hopefully be on the Desktop of the PC that's running Desigo CC. You'll need to shut down the UI, and stop the Project, and then shut the SMC. Launch the Update Desigo CC shortcut on the desktop > Click 'Next' > Then you should see an option to Modify the Language Packs (at the top right of the window). This will open a window to browse to and select the Language Pack. The language pack should be available from your Desigo CC installation media - simply browse to the Install Files\Languages folder, and select the fr-FR folder, and click Ok to add the new language. After this the new language should hopefully be available with the SMC under your Project. See link HERE. Regards, |
Last edited by: _CJ at: 01/20/2021 15:01:03 |
|
Follow us on