10/8/2019 9:17 AM | |
Joined: 6/28/2018 Last visit: 2/4/2023 Posts: 3 Rating:
|
Hello Guys, TIA-V15.1 SystemFunction: Program_Alarm. AlarmText Need to be changable at instance DB. See attachment PLC source program created by V15.1. Normally, alarm text can only change or define at FB Static. And if you go to instance DB, check the program_alarm type, alarm text is blocked/ gray-color, means, you can NOT change this. But this time, my attachment, you can see that program alarm text, color is white, means you can change the alarm text. My question is , how can this happen? how can I do to acheive same function?(change alarm text at DB) Thank you all. BR. AttachmentForSiemens.zip (138 Downloads) |
10/18/2019 10:08 AM | |
Joined: 6/28/2018 Last visit: 2/4/2023 Posts: 3 Rating:
|
OK, Finished & Solved. |
This contribution was helpful to
1 thankful Users |
7/24/2021 9:26 AM | |
Joined: 6/4/2018 Last visit: 3/6/2023 Posts: 1 Rating:
|
Would appreciate if you could share how this can be achieved, Thanks, Stefan |
12/15/2022 1:17 PM | |
Joined: 4/1/2022 Last visit: 12/15/2022 Posts: 2 Rating:
|
i've got the same problem, could you explain how you did it ??? |
Follow us on