4/1/2010 1:02 PM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928) |
Hello, My block icons from v7.1 are too big. Is it possible to set the property's of the block icons before they are generated? For example, the motor block icon has a width of 93, can I change it to 43, so that all the motor block icons are created with a width of 43? Or is the only way to copy all the icons to a template with @PCS7typicals (something like that) and c hange the prefix,change all the property's and then copy paste them back in the process picture? |
If I could help you, you can use the RATE button. Thank you. |
|
4/7/2010 8:53 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi You can modify alsothe standard-typicals (archive the orginal) and recomplie the OS, so you do not need to copy&paste all icons. regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on