11/16/2015 4:00 PM | |
Posts: 6 Rating: (0) |
Thanks Ste39, the protool panel is OP37 and will be replaced by MP277 panel. Best Regards |
11/16/2015 4:17 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello agutaya which PLC do you use.? if you have a PLC in Step7 V5.X then you can integrate the WinCC flexible Project into the Step7 and then when you connect them over an integrated Connection in Netpro you get the right Profibus Parameters and Settings for your connection If you use a manual connection in a not integrated WinCC flexible Project you have to compare the Settings manually. https://support.industry.siemens.com/cs/ww/den/view/38797080
Bye Murof |
If this Information really helps, you could use the Rate function |
|
11/16/2015 6:14 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, There is nothing to be downloaded into CPU. You should check the connection with CPU in the WinCC Flexible project. Kindly have a look at the following topic: Discontinuation of Production: SIMATIC OP37 |
Eng.Mohamed Ibrahim |
|
11/16/2015 7:17 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? |
Eng.Mohamed Ibrahim |
|
Follow us on