2/24/2022 7:33 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi mark, If you open the SQL Server Management Studio, please check under "Databases" if there is a database that is corrupt. It will be displayed in a grey background color instead of the orange background color. I had this problem several times when using VersionDog. Its an external application that copies the WinCC database to save user archives and log changes to the system, but sometimes this did not work properly ending up with a corrupt copied database and PCS7 would somehow disable charts and WinCC PC station in the project as well as a result. After deleting the corrupt database and a restart everything was fine. Maybe you got a corrupt database as well? The only thing is you cannot delete it since it is the project database and not a copied one in my case. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
2/26/2022 7:15 AM | |
Joined: 1/11/2019 Last visit: 4/23/2024 Posts: 684 Rating: (139)
|
Hello Mark, I was going through related query quite long before. I could find the query link, please go through the link given below. I might help you to some extent. If not please raise the service request. Query Link: Lost of Charts and Symbol table in PCS7 Service request link: Create service request |
This contribution was helpful to1 thankful Users |
Follow us on