12/14/2015 10:16 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello MrBin, The easy way is to use DP/DP Coupler if you have to exchange not more than 244 bytes of data Configuration of the I/O Data on DP/DP Coupler - ID ... |
12/14/2015 12:10 PM | |
Joined: 7/9/2015 Last visit: 5/13/2024 Posts: 3830 Rating: (557) |
Hi, here´s a FAQ for you, called "What are the special features of input/output addressing with the DP/DP coupler?" and the manual for DP/DP coupler https://support.industry.siemens.com/cs/de/en/view/22327981 Regards, Towome
|
|
|
12/15/2015 8:02 AM | |
Posts: 90 Rating: (0) |
Thanks about replies. I can directly communicate between 2 DP master S7-400 without using DP-DP Coupler? |
Follow us on