3/26/2015 11:53 AM | |
Posts: 9 Rating: (0) |
Hello guys, i am now working with CP 341 in CPU 315-2DP i almost did all programs in logic side and now i am working to communicate CP 341 (master) with WEST 6100+ controller .when i triggers the request bit the RLO goes till // "complete with error"// network and returns status event 16#e62 . i searched about this event in CP 341 manual for the cause and remedy . but i dont get that .i here giving some notes about the status and settings of my program CP 341 led status tx blinking rx blinking interface settings: baud rate: 9.6kbps parity :even stop bit: 1 slave device address : 1 Mode : RS485 (h-d) kindly help me with this issue am facing. its quite difficult to explain everything i did here but when i uploaded my program (10.8mb) its says attachment oversize regards, Anantharaman.N Nothing(k) is impossible if we think....
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/26/2015 1:59:28 PMNew subject after splitting |
|
3/27/2015 12:08 PM | |
Posts: 9 Rating: (0) |
this link will guide to my modbus master program cont..to my yesterday post 26.03.2015. sir but here i dont find that i have error in my slave address (1)as i have checked it again. sir to my personal view i thought that i having probelm in data types of db like source and work db . i here by attach the screenshots of my project DB's . kindly go through that and help me out . sir from modbus i have to access only two word parameters like setpoint and process valve . from west controller 6100 plus manual i found that the modbus access parameters are 1 for process variable and 2 for setpoint .so in my source db i converted the valve of 40001 to 9cf1 (hex). i getting send error codes like E62 after that i changed the datatype from byte to word my error code at that time be E32,E31 i having small probelm here only can anyone kindly help me out as i am struck out here for 48 hours of time. i also attach screen shots of my project.kindly suggest if anything went wrong my pgm link: https://www.dropbox.com/s/9sm0x0kbd5ybrmz/MODBUS_MASTER_PGM.zip?dl=0 |
Last edited by: AnantharamanN at: 3/27/2015 12:15:39 PM |
|
3/27/2015 5:47 PM | |
Posts: 3093 Rating: (322)
|
Hello Anantharaman, CP341 uses the addressing of the data link layer as defined in the Modbus specification. Address 40001 usually belongs to the application layer. Regards, |
Follow us on