12/2/2020 12:29 PM | |
Joined: 7/12/2016 Last visit: 10/5/2023 Posts: 4 Rating: (0) |
Good Morning!! I'm having trouble communicating a plc s7-300 as an i-device, and a PLC GE Rx3i as a controller. Do you have any example projects of these configurations? My intention is to read the information from the S7-300 on the RX3I. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/02/2020 14:42:55New subject after splitting |
|
12/3/2020 9:30 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
Hi andrelpn, There is an application sample: Configuration and Application of the PROFINET I-Device FunctionAlso this manual may help you: SIMATIC PROFINET System Descriptionin short:
after that, you can communicate over the projected IOs. No additional blocks are needed. hope this helps, regards, |
FCK WAR! |
|
12/3/2020 11:33 AM | |
Joined: 7/12/2016 Last visit: 10/5/2023 Posts: 4 Rating: (0) |
Another doubt, is it possible to transmit the internal variables of the plc, ex: MW, MD, M? |
Follow us on