Industry Online Support
Technical Forum
7/22/2009 4:16 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666) |
Hello Greg; The programming port of S5 CPUs uses a current loop (TTY)interface, so you need a converter cable such as this one,proposed by Siemens: 6ES5 734-1BD20 and a 9 pin to 25 pin convertor. I have not heard much success from USB to serial cables with this cable, unfortunatey. You clould also look at the offerings from another provider, but I cannot be certain that Step 5 is supporting them 100%: http://www.ibhsoftec-sps.de/english/Selection_Hardware_S5.htm Maybe someone else here has had a chance to use them? Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 7/22/2009 4:20 PM |
|
8/11/2009 7:24 PM | |
Posts: 28 Rating: (0) |
Hi, for my laptop which have only USB ports, I use an USB-RS232 converter produced by FTDIchip company. The type of my converter is US232R-10 Is working on XP Prof and Step5 V7.23. You can check the next link: http://apple.clickandbuild.com/cnb/shop/ftdichip?op=catalogue-products-null&prodCategoryID=84&title=USB-+RS232+%2B+DB9 dekor. |
9/24/2009 9:26 AM | |
Posts: 20 Rating: (0) |
hi Dekor does it works with you without any problem thx in advance |
Follow us on