Industry Online Support
Technical Forum
3/24/2008 7:53 PM | |
Posts: 4 Rating: (0) |
Helo, I´m trying to do the following: I need to communicate with Profibus PA devices to get status words from them and eventually send data to the device. I have a S7400 Cpu with Step 7, with a DP/PA coupler, and I don´t have Simatic PDM. So: If anyone can help me with one of these questions: 1)How do I communicate with a PA device, in order to get device status and send some data.(for example, the device http://www.astles.co.uk/001_pdf/download.php?filename=promag53_instr.pdf )(I need to use the device totalizer). 2)Is there any SFC, that does that? 3)How does it affect the bus baud rate and nodes? 4)Can anyone send me a example program, PLEASE! 5)Is there any program that simulates the device ? I dont have the device now, and I long as I know, the devices should only be arriving in the comissioning. You dont need to answer it all, any help is appreciated. |
Follow us on