8/1/2006 2:34 PM | |
Joined: 9/5/2007 Last visit: 3/7/2023 Posts: 317 Rating: (17) |
Hi, I don't think this can be done like you want. It's easy to create a recipe on TP1 and see the values on TP2. Just use the plc as a gateway and use PLC jobs to update the recipe values on TP2. The problem I can see is there is no way to build a list of recipe names on TP2 after they are created on TP1. Unless someone else has a different idea? It's maybe of no use to you but if the TP was TP177PN/DP then you could create the recipe on TP1 and use Sm@rtaccess to select the recipe on TP2. |
Last edited by: skimmer at: 8/1/2006 2:35 PM |
|
8/1/2006 4:32 PM | |
Posts: 3149 Rating: (171)
|
Hi, perhaps this FAQ can help? http://support.automation.siemens.com/WW/view/en/22777466 nemo |
7/13/2015 1:15 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
|