3/24/2016 10:40 PM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
what is the part number of communication unit (between two plc s7 1200) that is based on Ethernet cable RJ ? |
3/25/2016 7:54 AM | |
Joined: 2/2/2016 Last visit: 2/8/2023 Posts: 221 Rating: (2) |
I want to connect two plcs or more with a computer to do scada so I need switch. the port on the plc won't be enough |
3/25/2016 9:17 AM | |
Joined: 10/2/2013 Last visit: 6/4/2024 Posts: 339 Rating: (52) |
This may help you https://support.industry.siemens.com/tf/ww/en/postattachments/download/?attachmentId=25106 |
Technology is best when it brings people together,so we are here now :) |
|
This contribution was helpful to1 thankful Users |
3/25/2016 11:06 AM | |
Posts: 5225 Rating: (1188)
|
Hi Jeff. If you want to keep costs down and keep it in the Siemens family, consider.. |
This contribution was helpful to1 thankful Users |
3/25/2016 11:13 AM | |
Posts: 1529 Rating: (202) |
Thanks, let me check price/delivery. We have some strange delivery times here on some products. |
Follow us on