1/12/2017 2:52 PM | |
Posts: 2 Rating: (0) |
Hello, I need to communicate a PLC S71200 with RSView32 (PC Software). Is that possible? If so, I would like to know which protocol is possible to communicate, about the necessity to use a OPC server, and the hardware settings. Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/12/2017 3:48:40 PMNew subject after splitting |
|
1/12/2017 5:50 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Dear User,
RSVIEW is capable of communicating via an OPC interface with any automation product.For SIMATIC S7-1200 CPUs, you can check the following documents: How do you connect a PC station to an S7-1200 with OPC?
I hope it helps, HD Hosseini |
1/12/2017 8:14 PM | |
Posts: 2 Rating: (0) |
Of course it helps, thank you very much. now.. I am thinking about the hardware and the licenses I need to establish this connection. any suggestion?
|
Follow us on