2/24/2009 9:06 AM | |
Posts: 9 Rating: (1) |
Is there a tool to compare two FCT (script) files? |
2/24/2009 6:33 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi you can compare txt.files with the windows-function "fc". copy both txt-files to an folder. klick on the windows-start-button and on "run..." enter "cmd" in the dialog enter "fc file1.txt file2.txt > outputfile.txt /N" in the promt with "fc /?" you get the help of this function. Also there exsist a lot of freeware comparing tools. You can´t compare two functions in WinCC, as i know regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
3/10/2009 9:35 AM | |
Posts: 9 Rating: (1) |
Is there a tool to convert all *.fct files in the library directory to *.txt files? JBakkertje |
3/12/2009 9:16 PM | |
Joined: 4/21/2006 Last visit: 5/23/2024 Posts: 510 Rating: (24) |
Closed: This thread is closed, because the question is posted twice. You can find the other question here: Convert fct files. |