2/17/2010 10:27 PM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Hello Everybody I am looking for some information (FAQ) about comunication between PC and PLC s7-400 using Ethernet Ind. ISO. and CP443. Anybody has some information. Thank you |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
2/18/2010 6:26 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello JM76, Look at PC - S7 connections. Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
2/18/2010 9:51 AM | |
Joined: 9/19/2009 Last visit: 9/14/2024 Posts: 459 Rating: (85) |
Thank you Hristo Mihalev I´ve read this information and now I have a doubt! I am trying to download the project from the PC to PLC through ethernet network, but I have not set my PC to the Ethernet network. I try with a crossover cable, this is possible or I need to deploy to the network. thank you Regards J.Manuel |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on