6/6/2019 6:17 PM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating: (6) |
Hello! I have a PXC200ED where I have all the IO: BI, BO and AI modules in "configuration error". Is there any document where can I see what could cause this type of error. I have inserted all the address keys. I have the numbers from 3 to 16. I do not have 1, 2, 6 and 14. This could be a problem? Can a blown fuse cause this? Some of the leds where ligt up , so I assumed that the voltage is there. I have downloaded the program to the PLC whitout any problem. Thanks, Bruno AttachmentErros_AS_CT.xlsx (280 Downloads) |
Thanks, |
|
This contribution was helpful to1 thankful Users |
6/10/2019 11:32 AM | |
Posts: 1 Rating: (0) |
Dear Bruno, Did you cross-checked the io modules and their keys with CFC. |
Follow us on