6/10/2006 6:56 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi Dimbas, With the masterport you can do the FMS-communication to the 2 SIMATIC S5 PLCs, with the slaveport you can make the S7-317 the master. There is a example on the Net, i have found it under ID http://support.automation.siemens.com/WW/view/en/6167688 (Siem80b4.gsd seems to be the gsd-file for the CP5614 Profibus DP Slave port.) But i couldn't find it anywhere [:cry:] There are several demo and handbooks on the net that describe the function of the CP5614. 13542666 Commissioning PC Stations - Manual and Quick Start 2005-05.pdf 13664901 CP5613 CP5614 CP5613 FO CP5614 FO CP5613 A2 CP5614 A2 2003-11.pdf 1653531 SIMATIC NET DP Base Programming Interface for CP5613 CP5614 2001-07.pdf See also the examples in the DP Development Kit in Siemens DP 5614. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
2/12/2007 2:38 PM | |
Posts: 7 Rating: (0) |
Hi everyone, I've found siem80b4.gsd in the "gsd" folder in the CPBV51 folder (Com Profibus V5.1 install folder) Here is it joined. I didn't test it but I will. Regards AttachmentSiem80b4.zip (717 Downloads) |
Follow us on