7/8/2022 8:34 AM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating: (930)
|
Hi, Did you do the following procedure? In WinCC explorer you insert a button, select it and via the dynamic wizard you select: SFC->Configure SFC Button. You then select the correct SFC instance, after that the view you want to open and finish the wizard. What you can do is open "apdiag" on the OS. Its a tool that monitors script behavior. You can find it under: C:\Program Files (x86)\Siemens\WinCC\uTools and select apdiag.exe. When opened, click on Output Window->Open and then press the button. You probably get a result in the output window, you can post it here. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on